Hi All,
I would like to ask one question about OPA357AIDBVT footprint.
I downloaded PADS-PowerPCB footprint from http://focus.ti.com/docs/prod/folders/print/opa357.html, and measured the distance between outer edges of pad 1 and 6, which is 3.6mm.
But on page 23 of SBOS235E, the OPA357/OPA2357 document, for DBV (PDS0-G6) the corresponding distance is [min: 2.6, max: 3.0], with max smaller than 3.6mm.
I cannot find mechanical for “DBVT” in the document.
So am I getting the right footprint file?
Thanks,
Zheng