Part Number: LMH6642
Other Parts Discussed in Thread: LMP7731
I just ran into a problem that I can't quite figure out the cause of.
The LMH6642 is wired as shown below. The primary function of this circuit is to buffer a reference voltage, the secondary function has AC characteristics.
R110, R111 and C83 serve as external compensation. The OpAmp is stable.
VBRGP = 2.5V DC.
The LMH6642 datasheet gives an input offset average drift of typ. +/- 5uV/°C.
However, measurements I made myself in the oven give values up to 100 times the specification (500uV/°C).
The exact same circuit with the LMP7731 behaves correctly.
What have I overlooked in the design with this OpAmp or is this behavior known?
Regards Bernd