Part Number: INA3221
This part is in a QFN16 package with a Thermal Pad on the bottom (EPAD).
Can the Thermal Pad be connected to GROUND?
The datasheet does not say explicitly if the EPAD can be connected to GND.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA3221
This part is in a QFN16 package with a Thermal Pad on the bottom (EPAD).
Can the Thermal Pad be connected to GROUND?
The datasheet does not say explicitly if the EPAD can be connected to GND.
Russel,
Yes, the thermal pad of the device can be connected to GND. This is how the device is configured on the EVM.