I am trying to use the OPA145, but I get this error message as part of the report when simulating.
There are errors in the circuit. Simulation aborted
OPA145.lb (333): .param Gain = 1e-3
*** ERROR *** Illegal subcircuit reference - 'IC4.XIQ+'.
The characters: ' ()^+-*/,&|='
may not be used to call a subcircuit that uses parameters
I have attached the file for the OPA145, which came from TI.
If you look at line 333 you will see the errors.
I can supply the rest of the correspondence about this if required.
It was sent to our spice technical support
With kind regards,
Ernest