This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLC2201AM-MIL: Difference between TLC2201AMJG and TLC2201AMJGB

Part Number: TLC2201AM-MIL


Hi TI expert

Could you tell me what is the difference between TLC2201AMJG  and  TLC2201AMJGB?

Thanks and Best regards,

Thomas

  • Hi Li Chen,

    I do not have all the answers for you currently. I have to ask our engineers who are familiar with the markings in the product.

    Here is what I found out so far. 

    1)      “B” Grade is 100% tested for noise figure. The B grade is higher grade, which it has lower noise specification, see the captured image below (I was told that A grade was also 100% tested in noise figure, but I need to reconfirm the information tomorrow.).        

    2)      Marking for TLC2201AMJG and TLC2201AMJGB will be different , see the image below. 

    3)      “M” suffix denotes device is characterized for operation over military temp range, which is defined in the datasheet. 

    TLC2201AMJG should indicate A grade, TLC2201BMJG should indicate B grade. However, I have not found out the definition of last letter "B" stands for. I will update the information for you tomorrow, when I have it. 

    Best,

    Raymond 

  • Hi Raymond 

    Thank you for you replying.

    Waiting for your update information.

    Thanks and Best regards,

    Thomas

  • Hi Li Chen,

    I am still working on your request, except I have to find right engineer or department to get the relevant device marking information.

    All TLC2201AMJG (A grade) and TLC2201BMJG (B grade) devices are 100% tested for noise specification. We believed that the last letter designation in  TLC2201AMJGB device marking may have something to do with a specific process requirements to meet the Mil-compliance. Sorry for the delay, and I will post the information as soon as I have it. 

    Best,

    Raymond  .  

    .

  • Hi Li Chen,

    As we previous indicated, TLC2201AMJGB part is "A" grade part, and the part with added B suffix means that the all processing, screening, quality conformance and inspection are in conformance with MIL-STD-883 test method standard. 

    If you have additional questions, please let me know. 

    Best,

    Raymond