Part Number: INA303
Hi,
The customer has constructed a circuit using the INA303A2.
1. Please check if there is any problem with the configured circuit.
Current Sensing Circuit_INA303A2.pdf
The battery voltage is input at 400V, so please check whether it can be connected to the sensing part (IN+, IN-).
2. If the potential difference between both ends of the sensing resistor is 50mV or more, can a defect occur?
Thanks.
Regards,
MJ