Part Number: INA226
Can VS be supplied by VBUS?
In that configuration can I measure the INA226?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: INA226
Can VS be supplied by VBUS?
In that configuration can I measure the INA226?
Thanks
Hey Kevin,
Thanks for posting to the forum.
VS can be supplied by VBUS as long as VBUS is always less than 6V, which the Absolute Maximum voltage allowed at Vs pin. In order to monitor the quiescent current (IQ) of IN226, the VS pin needs to connect in parallel with whatever load your may be sensing. So if the load is connected to the IN- pin and your are measuring positive current (Vshunt>0), then Vs also needs to connect with IN- pin. If Vs is connected to IN+ pin in this scenario, then you will not sense this current since it is not flowing across your shunt resistor.
Best,
Peter
It depends on what else VBUS is connected to. If VBUS can have transients like load dumps, inductive loads, etc., then it'll eventually destroy the ADC, or at least will be progressively degrading its performance. I'd probably not use VBUS if it leaves the board, i.e. if there's a physical connection from VBUS to points outside of the PC-board. Even ESD will be a concern if VBUS leaves the board. It'd take a bit more knowledge about the specific VBUS "environment" to say how good of an idea it would be. Meeting the absolute voltage limits statically across the operating temperature is the basic requirement too, of course.