This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA2626: OPA2626 PSpice very strange results

Part Number: OPA2626
Other Parts Discussed in Thread: OPA626

Hello,

I'm simulating a simple noninverting circuit with the OPA626 in OrCAD PSpice 17.2. It runs fine, if the voltage at the +Input is 0.5 * (VCC-VEE). If it deviates by an offset from this (for instance by 150 mV), I get very strange results in transient simulation (see appendix). AC simulation doesn't give any useful result anymore.

I would like to have a working PSpice-Model of the OPA626.

Regards!

Andree

Transient.pdf5633.SCHEMATIC1 _ PAGE1.pdfOPA626-Test-PSpiceFiles.zipOPA626.lib