I'm using a TI LT1013 op-amp to process the current through a 50 mV shunt. I'm having some issues with the op-amp not performing well in certain conditions and I'm not sure why.
It seems that the output of the opamp does not follow the input although the inputs are with Common mode range and the outputs should be well within the rails. The issue happens mostly at higher current values. Any ideas on why it is not operating correctly?
I attached the schematic section I use.