Other Parts Discussed in Thread: INA226
Does ina226 provid in space RAD 100 package?
Or can you provide a similar device with RAD HARD 100?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: INA226
Does ina226 provid in space RAD 100 package?
Or can you provide a similar device with RAD HARD 100?
Ramin,
Unfortunately we do not currently offer a digital power monitor such as the INA226 in a radiation hardened offering. We only have analog devices as of today. Our two current shunt monitor offerings are:
- INA901-SP is our fully RHA device. It is Radiation Hardness Assured (RHA) at 50 krad(Si) at Low Dose Ratem and is Single Event Latch-up (SEL) Immune to 75 MeV-cm2 /mg at 125 °C,
- INA240-SEP is SEL Immune to 43 MeV-cm2 /mg at 125°C, and is ELDRS Free to 30 krad(Si) – Total Ionizing Dose (TID) RLAT for Every Wafer Lot up to 20 krad(Si)