I can't find in the datasheet how much load current the amplifier pin 8 output in can handle, or it's internal output impedance. Can only find it's maximum capacitive load is 1nF. Need to know, because the connected sampling ADC have some demands on maximum source impedance, and also I would like to filter the current just before the ADC with an RC-filter, therefore I would need to know this data.
Best regards/ Johan Olofsson