Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA837: Possible errors in the max output current section

Part Number: OPA837
Other Parts Discussed in Thread: OPA838, OPA2837

I was going to use this table in an article discussing max linear output current - might be a few errors here, this is in the 5V table, 

1. Perhaps the overtemp output voltage swings should be at gain of 2 not 5? I get the top line specs, this output voltage swing is into 2kohm load, but to be completely accurate at gain of 2, you need the feedback R to set that Rf+Rg parallel load. 

2. Not stated, except at the top as a 5V supply, but these are clearly +/-2.5V specs for the output current lines - might need to add that to the conditions

3. Did not look, but 3V table might have similar issues

4. Did not look, but the OPA838 and OPA2837 might have similar issues.