Part Number: THS4561
Other Parts Discussed in Thread: THS4551
Still wandering for good linear output current examples - Had hoped the THS4561 would be it for this audio article, not at this point,
Here is an earlier THS4551 continuous output current on 5V, can kind of make sense of this, and yes a +/-2.5V differential will work on single supply as each ouput swings around 2.5V +/-1.25V. I guess I will use the THS4551 for the article as the THS4561 is too messed up.
The THS4561 is a perplexing,
1st the spec tables have collapsed to 5 to 12V range, fine but the part was designed for 3V operation and there are curves at 3V, what happened to the 3V specs?
Also, for the linear current output, where is the load - you can solve for it of course, but should be listed there, and on the continuous output current spec line, what is the supply.