Part Number: INA302-Q1
Hi,
We are using INA302A3QPWRQ1 in the design. Please provide response for the below queries
1)How the offset voltage varies with temperature? Whether offset voltage increases with temperature or vice versa? The value provided is positive (0.25uV/C), so can it be considered that offset voltage increases with increase in temperature?
2)How the gain error varies with temperature? Whether gain error increases with temperature or vice versa? The value provided is positive (10ppm/C), so can it be considered that gain error increases with increase in temperature?
3)How to include non-linearity error in the calculation? Whether it can be added with gain error?
4)In the datasheet pgno:6, internal programmable delay error is provided. Where this "internal programmable delay error" term will have an effect? Whether it will affect the delay time set by external capacitor? If so, what is the formula to calculate the same?
5)Whether Vout pin can be left floating?
6)In the datasheet pg no:5, recommended differential voltage is provided as 25mV. In our design, differential input voltage is coming around 27mV. Whether this recommendation can be violated?
Thanks
Viswa