Other Parts Discussed in Thread: INA326
Hello,
I use INA326EA in the pressure transducer conditioning circuit with following settings:
- Gain = 0.5 resistors according to datasheet recommendations
- Supply Voltage = +5V single
- Vin+ = +0…4V, normally 2.5V
- Vin- = + 0…0.5V
- Decoupling capacitor 0.1uF
- Output filter 100R, 1uF
Sometimes at power-up the output permanently goes to positive rail with 0.2V ripple on it. The root cause of the problem is oscillation ~ 150kHz on pins 1 and 8 (gain setting resistor).
The problem is intermittent; not all boards exhibit this problem.
Please advise.
Regards,
Vlad