Other Parts Discussed in Thread: RCV420, XTR111
Most industrial interfaces use the 4-20mA interface as a discrete interface to represent 0s and 1s with those two levels. I need to have an interface to a 4-20mA input, that can vary at least 1.6mA increments from 4-20mA. 4mA represents a off state, and 20ma is a full on state, and I need to be able to vary throughout this range, with fairly course steps. I would rather have 0.8mA increments throughout that range to give me better resolution. Is the load looking into a 4-20 interface standard? Is it resistive at a fixed load? I'm not familar with this type of interface. I assume I need a voltage source, perhaps a DAC, and then a current driver of some sort. Any help will be appreciated.