Other Parts Discussed in Thread: INA220, INA282
I
have an INA220 designed into a product that now needs to accommodate a
voltage of 28V at the VBUS, VIN+ and VIN- pins (high side current
sense). I have unused component locations for resistive dividers on all
of those inputs. I tried using pairs of 40.2K 0.1% resistors to divide
down the differential voltages from the current sense resistor. With a small current (20 mA) through a 0.01 Ohm resistor the voltage
differential at the VIN+ and VIN1 inputs was about 0.4V - much larger than expected. The original circuit (without resistive dividers) used 10 Ohm resistors in series with the VIN+ and VIN- pins of the INA220 and worked just fine. The input circuitry to those pins is symmetrical and within
0.4" of the input pins of the INA220. In an effort to understand what is causing the large differential voltage I removed the halves of the resistive dividers going to ground, so the circuit is the same as my original circuit, but with 40.2K Ohm resistors instead of the original 10 Ohm resistors in series with the VIN+ and VIN- pins of the INA220. I reduced the applied voltage to 24V. The large differential voltage is still across the VIN+ and VIN- pins of the INA220. This seems to imply the input impedance of the VIN+ pin is different than that of the VIN- pin. Is that the case or am I overlooking something? I consulted the data sheet and it specifies the same input impedance for both the VIN+ and VIN- pins: 20 uA, Can anyone explain why the input impedance is listed in units of uA? Thanks.