Part Number: OPA455
Other Parts Discussed in Thread: INA149, INA146
Hello there,
We are using the OPA455 in an improved Howland current source topology. Our goal is to be able to deliver +/-2mA to a maximum compliance of +/-75V. I had a few questions:
1. The quiescent current of the OPA455 is rated at 3.2 - 3.7mA when Iout=0mA. We are using +/-75V at the rails, so a maximum VDD-VSS = 150V. We will supply a maximum of 2mA peak to peak at the output load. What is the right way to estimate the power consumption/efficiency of this chip with this information?
2. Do you have suggestions on any alternative options to have a lower quiescent current for the same application?
Thanks!
Ashwati