Other Parts Discussed in Thread: LM318, TINA-TI
Normal 0 0 2 false false false MicrosoftInternetExplorer4
Hi,
I am looking for an Op Amp to precisely follow up the input signal. The Op Amp
is apply as an inverter and the input voltage is around 20mV~100mV with 300kHz
frequency. The gain will be set to 100 when using 9V~12V single supply voltage and
anticipate the output to be precisely without any delay. In my hand, I am now using
LM318P which is an high speed Op Amp, but the output signal would distort when
apply at such setting. Can anyone suggest any Op Amp with low quiescent current
which price is below 1.00 | 1ku. Thanks.