Part Number: ISO224EVM
Other Parts Discussed in Thread: ISO224, OPA277, AMC3330
Now I use iso224evm to test, the front-end uses 100A: 3.53v transformer to sample, and the signal is sampled to ADC through iso224 and opa277 amplification circuit;
The connection is as follows: iso224evm, VDD power supply ± 12V, VDD2 power supply + 5V, vdd1 power supply + 5V / external input + 14V through tps74050 on board. It is found that TP3 output of iso224 output test point is 2.22V DC when there is no output, 50Hz / 560mv signal and 1V signal from transformer output. The input and output waveforms are as follows:
Please help to analyze the reasons?