Part Number: OPA2171
Other Parts Discussed in Thread: OPA2991
Hi team,
Could you please help us review below customer's OPA2171 circuit schematic? The high value of resistors provide isolation function here.

Best Regards,
Stanley Dai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Stanley,
Why is the customer not using the OPA2991 instead?
The customer has switched in IN- and IN+ connections. This means they are using positive feedback! They need to switch the connection so the feedback connection connects to the IN- input.
They also have the positive power supply pin connected to GND and the negative power supply pin connected to +5V. This will damage the device! The positive power supply pin should connect to +5V and the negative power supply pin should connect to GND.
Is there a capacitor at the Isense node? Once I have this information I can perform a stability analysis for you.
Lastly, the output will not be able to swing all the way down to 0V with a 0V input due to the output swing limitations of the device.
Thank you,
Tim Claycomb