Part Number: LOG112
Other Parts Discussed in Thread: LOG104, LOG114, LOG101
Hello everybody,
I want to use a logarithmic amplifier (LOG104, LOG104, LOG112, etc) but it seems that there is some discrepancies about le log conformity error calculation in volt.
I found the LOG100 original datasheet where the error calculation seems to be best described but there is always something that I doesn't understand well.
The non linearity is given in Volt with the formula:
VOUT (NONLIN) = K 2Nm V
Where K is the gain of the amplifier (V/dec), N the log conformity error and m the number of decade.
But Why there is this factor of 2?
In the specification table, in all the datasheets, the log conformity error is given relatively to the full scale peak to peak output. The mention "peak to peak " disappeared from the TI datasheet in the log conformity chapter so we could think that we need to take the one sided full scale value (by dividing the value given in the table by 2?).
Where is the truth? is the value in the table not peak to peak? Or if somebody is able to explain me where the factor of 2 come from?
Best regards,
Wilfrid