Other Parts Discussed in Thread: THS4081, OPA810
Hi,
The metal detector project will need to design-in stable oscillator circuits with related discrete components(op-amp, inductor, capacitor, and resistor).
The oscillator’s basic specifications and requests are listed below.
1, The oscillator can generate a stable sinewave signal only with 100Hz ~ 1MHz bandwidth.
2, The oscillator needs to have stable/fixed sinewave amplitude output with 14.4Vp-p(peak to peak) or 5.1Vrms within the full band(100Hz ~ 1MHz) based on dc +/- 8V dual power supply.
3, The oscillator’s positive feedback networks must be designed with both inductors and capacitors only(NOT resistor and capacitor).
4, Please also recommend the single channel OP amp from TI.
And there are two additional key requested specifications of this oscillator design as below.
1, Condition one: If the oscillator is working under “200K Hz operating frequency”, please provide me all the component values/specifications settings of this oscillator.
2, Condition two: If the oscillator is working under “1K Hz operating frequency”, please provide me all the component values/specifications settings of this oscillator.
Regards
Rock