I would like to know whether AFE5807 can be used as an analog front end when Capacitive tranducer (CMUT) is used in place of conventional piezoelectric transducer. I understand that the AFE 5807 is typically used with Piezoresistive/electric transducer where in the input is a voltage. Incase of CMUT transducer, output is a current and traditionally the interface circuits are either TIAs or charge amplifiers. If AFE5807 is not suitable, can anybody recommend an appropriate device (Opamp/TIA) for my application. I have a 2D array of transducers and the Signal band can be from 500KHz to 50MHz .