Hello Guys,
Good day.
Thanks in advance!
Art
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Guys,
Good day.
Is there any available Spice model you can share to use for this device? If you can suggest any other methods of modeling it. Maybe a similar PGA or different software?
If we are to request for a model be created for this device, is that possible? Because I know there are some devices where spice models are not possible.
Thanks in advance!
Art
Hello Art,
The PGA309 device was developed and introduced to the market more than a decade ago in 2003, and therefore no SPICE model was developed for the device. The best way to get familiar with the device is by using the PGA309EVM-USB evaluation board. The PGA309EVM-USB GUI/software includes an auto-calibration algorithm that selects the optimal gain and offset adjustment settings for a given sensor and output target requirements. The hardware also includes a sensor emulator that allows to program sensor characteristics to emulate the sensor hardware. The GUI also offers a "Block Diagram" tab that allows the user to experiment with settings. Attached find some EVM information links and power-point that can be useful. If you have further questions, please feel free to contact me directly via email.
Thank you and Regards,
Luis
PGA309 Device User's Guide:
PGA309 User's Guide (Rev. B) (Device User's Guide)
PGA309EVM-USB information:
PGA309EVM-USB User Guide (Rev. B)
Power Point Presentation: Use USB_DAQ to Complete the Calibration of PGA309 EVM