This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA380: Can OPA380 used to amplify the photodiode which is illuminated by a DC light

Part Number: OPA380


Hi Guys,

Good day. We need your help to check our customer's concern.

I have attached OPA380 TIA circuitry that was used in two cases from our customer. Kindly review the circuit.

Currently they are using the OPA380(single-side power supply +5V, pin-4 is to GND) to convert and amplify the Photodiode's photocurrent. The PD is illuminated by a LED biased with a DC voltage. However, they can only get a constant voltage around 3.4V with a 1 Mohm feedback resistor and no feedback capacitor each time under different LED light intensities. The output voltage is supposed different because the PD photocurrent is different under different LED intensity.

When they use OPA380 to amplify the PD' photocurrent which is generated by shining a AC modulated LED (e.g. a squre wave), the photocurrent in that case is AC and OPA 380 works well there and can generate a square voltage output.

In the first case from customer photocurrent is DC. Some Transimpedance Amplifier (TIA) does block the DC current (so-called DC current rejection). Kindly confirm if it is true that OPA380 also blocks the DC current if PD is shined by a light source with constant light intensity? Or there is something wrong with the connection. 

Looking forward to your response. 

Best regards,

Jonathan