Part Number: TLV7041
Other Parts Discussed in Thread: TLV7031, TLV9032, TLV9022
I have built an inverting comparator circuit in TI Tina. I copied the circuit from the TLV7041 data sheet (SLVSE13G – SEPTEMBER 2017 – REVISED DECEMBER 2020- page 20-21). The circuit is for a TLV7031! I believed that it would work using the TLV7041, but I needed a pull-up resistor on the output.
The circuit is designed to compare the reference voltage of 5V to the input (neg). The High to Low trip voltage is 3.33V and the Low to High trip voltage is 1.67V
The circuit output does not change state at the trip voltages, using the pull-up resistor. Removing the pull-up, the output is around 2V, not the 5V reference voltage that I expected.
I have attached the circuit.