Part Number: OPA392
Other Parts Discussed in Thread: OPA333, , OPA325, OPA391, OPA376
Hello,
I have an existing design that uses a low GBW amp (OPA333) in DCK (SC-70) package to drive an ADC. It works OK at very low sample rate but I now want to sample faster so am looking to find something with higher GBW (>8MHz) to replace it.
Ideally I'd like a direct replacement. The OPA325 would have been ideal but it's only available in the larger SOT-23 package and, even if I was able to update the bare board, it's so tight that I'm not sure I could fit it in. The new OPA392 looks a very nice amp from the datasheet and very appropriate as an ADC driver. Datasheet says part will be available in DCK package.
I know it's only at the stage of initial samples being available just now, but any idea as to when something in DCK package might be available? I'd like to include it in my design, but it depends how long I'd have to wait.
Thanks,
Gordon.