Part Number: INA240
Other Parts Discussed in Thread: INA168, INA302, INA293, INA303, INA290, INA301, INA138, INA280, INA281, LMP8640
I would like to use this part to sense inductor current connected to switching point of half-bridge, in a high-frequency(up to MHz fsw) power converter. Would like to consult:
1.If the current ranges from 0A to 50A, how much shunt resistance do you recommend? And how to evaluate its output accuracy when current approaching to 0?
2.What is the special reason why this part has very good PWM rejection?
As in my understanding, if it is connected to switching point, good high-frequency CMRR OP-AMP is needed to deal with switching glitch. Does it mean this part has a very good high-frequency CMRR OP-AMP, along with well-matched resistance inside?
3. Do you have similar parts but with much higher bandwidth(up to MHz)? Could I understand that the PWM rejection functions have bad impacts on dynamic performances?