Part Number: TLV7032
Other Parts Discussed in Thread: TLV7031, , TLV1701, TLV7041
Hi,
I'm trying to simulate a window comparator with the TLV7032. I have tried using both the TINA model for TLV7031 (x2) and the model linked in this previous question (https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/902742/tlv7032-tlv7032-simplis-model-or-tina-model-request?tisearch=e2e-sitesearch&keymatch=tlv7032#). Neither model is giving the expected behavior.
For simplicity, if I set the VCC rail at 3.3V and use three equal resistors to form the two thresholds, as in the basic example in the datasheet. The swing on the output is only ~0.01V (see pictures and attached TINA schematic). Is there an issue with the simulation model? Is there something missing from my simulation?
I have gotten the same simulation running as expected with the TLV1701 model, which is what makes me question if there is a bug with the 7302 model.monitor1704.TSCmonitor7304.TSC