Other Parts Discussed in Thread: TIDA-01040, OPA827, INA128
Hello,
I am trying to do transient analysis with TINA-TI and keep getting the error "Convergence problem. Check the analysis parameters!"
What can I do to solve this?
Thanks,
Adam
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am trying to do transient analysis with TINA-TI and keep getting the error "Convergence problem. Check the analysis parameters!"
What can I do to solve this?
Thanks,
Adam
Hi Adam,
It looks like you're trying to simulate the TIDA-01040 reference design. The transient sim does not appear to be modified from the original version (here). The sim seems to be locking up because something in the OPA827 model is unhappy. I ran the unaltered transient sim that is included with the other TIDA-01040 simulations and saw the same error occur.
I was able to fix it by including a 10.5 ohm resistor between the output/feedback of the OPA827 and the 1.5k resistor. This resistor appears in the schematics on the reference design page but is missing from the sim. Once the resistor was added, the simulation did converge, although it took some time to do so. After getting it to run with the 10.5 ohm resistor I added the 10pF cap and it again converged.
I'm not very familiar with the OPA827 or its model, so perhaps someone from the high-speed group can weigh in with more details as to exactly why this occurs.
Cheers,
Jon
Hi Adam,
it's the usual mistake: TINA-TI does not like too many OPAmps running in one simulation. So, as you know what the output signal of INA128 will be, divide and conquer:
Or by other words: Divide the whole circuit into individual sections and simulate these sections separately
Kai