Part Number: LM2907-N
Hello,
On page 4 of AN-162 I believe there is supposed to be an equation for selection of R1.
It seems to be missing, is anyone able to provide the equation or update the file?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LM2907-N
Hello,
On page 4 of AN-162 I believe there is supposed to be an equation for selection of R1.
It seems to be missing, is anyone able to provide the equation or update the file?
Hi Lester,
Certainly the equation for C1 can be transposed to solve for R1, but you would need to have a value for C1 already established. Note that prior to the C1 equation being presented in the AN-162 section "Choosing R1, C1 and C2" there is discussion about three criteria with regards to selecting R1's value. Once they are considered and a value is for R1 is decided upon, that is when the C1 equation is provided which includes the decided upon value for R1. Following this procedure helps better set a C1 value for more optimized performance from the LM2907-N. Once R1 and C1 are established, then C2 is determined from the C2 equation.
If you go through the LM2907-N datasheet you will notice that many of the circuits and examples provided use an R1 of 100 kilohms. That appears to be a value that satisfies a wide range of the applications to which the LM2907-N is applied. However, it is best to follow the three R1 selection criteria in AN-162 and find the value that best fits your application.
https://www.ti.com/lit/ds/symlink/lm2907-n.pdf
Regards, Thomas
Precision Amplifiers Applications Engineering