This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO121: PSPICE Model Netlist Errors with PSPICE for TI

Part Number: ISO121
Other Parts Discussed in Thread: ISO224, ISO120,

PSPICE for TI comes with ISO121X Model and when using it to simulate a simple application circuit, it results in several netlisting errors as shown below and simulation does not run, this is the same case with ISO120X model also, are there working versions of ISO120/1/2/4 (or ISO224) which can be used with PSPICE for TI? Information about the error is attached below:

INFO(ORCAP-2191): Creating PSpice Netlist
INFO(ORNET-1041): Writing PSpice Flat Netlist C:\Users\...\Documents\PSPICETI\ISO121X-PSpiceFiles\SCHEMATIC1\SCHEMATIC1.net
ERROR(ORNET-1019): Pin 3 in template not found on U1
ERROR(ORNET-1019): Pin 4 in template not found on U1
ERROR(ORNET-1019): Pin 17 in template not found on U1
ERROR(ORNET-1019): Pin 18 in template not found on U1
ERROR(ORNET-1019): Pin 19 in template not found on U1
ERROR(ORNET-1019): Pin 20 in template not found on U1
ERROR(ORNET-1019): Pin 21 in template not found on U1
ERROR(ORNET-1019): Pin 22 in template not found on U1
ERROR(ORNET-1019): Pin 23 in template not found on U1
ERROR(ORNET-1019): Pin 24 in template not found on U1
ERROR(ORNET-1019): Pin 37 in template not found on U1
ERROR(ORNET-1019): Pin 39 in template not found on U1
ERROR(ORNET-1019): Pin 40 in template not found on U1

PSPICE for TI Version: 2021.1, TI Models and Libraries are updated

Thanks and Regards,

Vaishnav