Part Number: OPA4187
Other Parts Discussed in Thread: OPA187
Hi Team,
If the (noninverting) input (pin 2) gets a voltage in the range of +/- 2,4 .. 3,5 V I see a corresponding output as expected only in the negative range. The positive voltage is limited to appx. 2,4V even if the input is above 2,4V. could this behavior caused by a non-connected Thermal Pad?
Thank you.
-Mark