I am trying to communicate with a TAS5717 using I2C without any luck. The +3.3v supply seems to be correct and another device (EEPROM) on the same I2C bus is working ok.
The reset and power down pins are both high. I have tried both addresses 0x54 and 0x56 and the first byte of the I2C message is not ACKed by the 5717. I have looked at the SCL and SDA signals at the chip and they look fine, with a 0 to +3.3V voltage swing.
Is there something I am forgetting?