Other Parts Discussed in Thread: TPA3255
Hi Sir
Does TI have similar output watt solution with TDA7498E
OCP 11A when Rload=0ohm (0ohm is necessary)
(TPA3245 is 13.5A when Rload=1ohm)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Justin
This is a special application .our end customer use TPA3245 to driver a transformer and the structure like below
When test with TPA3245
1. BTL Mode(INA+INB)
2. Input Sine wave 1.2Vrms ,the CLIP_OTW LED will indicate and this moment the output voltage is under 10Vrms
3. At the same condition ,TDA7498E is workable
So I guess TPA3245 is OCP ,do you have any suggestion or others solution can replace TDA7498E?