This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am analysing failure modes on a product (4-20mA application) that use the XTR115.
I have measured about 26-30 ohms between pin 3 and pin 4 of XTR115.
However in modules that have failed, I have noticed the measurement to have changed (to anything from 0 to mega-ohms).
Please advise: What is the tolerance for the value, in the datasheet it is shown as 25ohms.
Please advise: What could cause this value to drift up or down.
Thanks for your response.
Here I further elaborate on the problems we are experiencing.
Failure mode: The unit(s) randomly stop generating the (4-20mA) loop current.
In our returned products lab, we have elected to measure the resistance value between pin3 and pin4 in order to determine the health status of the XTR115. It is a parameter that can be accessed while the component is in circuit.
Our findings so far show the resistance to change( 0 ohms to Mega ohms). The change can be permanent or momentary.
In cases where the change is permanent:- The loop current becomes disproportionate to input or disabled.
In cases where the change is momentary:-
After a series of testing (power-cycling), the measured value returns and stabilizes at 31ohms.
These units have been returned for dropping out (No loop current, while everything else is on).
In our tests as manufacturer, the units are giving correct loop current.
In your response, please include advice on the following.
Thank you Kai and Zak.
We are setting up a series of tests that take into your valuable advice. I will update you with our findings.
In the meantime,..
Please advise the expected time to failure of the XTR115 when it is run in the following mode
Thank you for this advice.
We indeed have functional earth connected to Pin3. Our Engineering team is going to avail me some schematics to share with you.
May I highlight to you that failures are being reported after 12months of product being in service.
There are some further points that we need to clarified:
From Zak Kaye
…..maintaining the proper ratio between R1 and R2. You may see a shift in this value of +/-20%, but the ratio will be very accurate.
…..The momentary case is much stranger. If your loop supply dips heavily then the loop may be out of compliance for the XTR. Are you using an external transistor or relying on the internal transistor? If you use the internal transistor or an external transistor placed too close to the XTR then this could be a thermal issue. Understanding the conditions in which this occurs can help eliminate this as a variable. Does this typically manifest at higher output current levels?
Hi Victor,
you need functional earth being connected to pin 3? Oops!!! Not good!! This is the cause for the failures! If possible, connect functional earth to pin 4 and not to pin 3. If not possible, change the circuit! Connecting functional earth to pin 3 will damage the chip again and again!!
Kai
Hi Victor,
even if the 24VDC supply is labelled "isolated" there's always stray capacitance between the 0VDC terminal and mains voltage! This can be the interwinding capacitance between the primary and secondary winding of mains transformer or the interwinding capacitance of the switch-mode-supply's transformer. This stray capacitance to mains voltage can be up to 10nF very easily. And if there's a surge of some kV on mains voltage, and you have dozens of them every day, a current is running through this interwinding capacitance and through the connection between pin 4 and pin 3 of XTR115 to the earth terminal of your PSU block!
This will kill the XTR115 sooner or later!
Kai
Thanks once again. Currently our engineering team have very little roam to change the design.
A minor change to the deign that has been accepted is illustrated below. A resistor (R3) is placed between Pin 3 and 0V(earth). It is hoped the resistor would provide some kind of isolation of Pin 3 from earth. We have done some tests and managed to get correct output loop current. Do you foresee any problems with this proposed change.
Hi Victor,
at first sight, this seem to be a good solution. The current between pin 3 and pin 4 is limited by the inserted 6k8 resistor and should no longer destroy the chip.
But, unfortunately in the situation of a surge it will kill the XTR115 now due to a massive overvoltage between pin 3 and pin 2 of XTR115. This can be seen from the following picture:
Even if only 1nF stray capacitance (interwinding capacitance) to the mains voltage is assumed in the 24V supply on the right, a massive overvoltage will occur at your 6k8 resistor during a surge.
A surge is an overvoltage pulse of about 1.2µs rise time and about 100µs fall time. In the CE standards it is coupled between the mains voltage and earth. e.g., has a peak voltage of 2kV then and is current limited by 12R. In the following you will see a simplified surge analysis:
It can clearly be seen that for a brief period nearly the full peak voltage is dropping across your 6k8 resistor, while the voltage at pin 2 is clamped to about 4.7V. This will cause a massive overvoltage between pin 3 and pin2 of XTR115.
Another disadvantage of the 6k8 resistor is that every mains noise is directly coupled into the signal path now, because of the voltage drop across the 6k8 resistor.
So, I would strongly recommend not to insert such a resistor. I would try a diode clamp between pin3 and pin 4 as shown in the following picture:
Using 1N4001 diodes for the clamp should be adequate. The needed current rating can be estimated from the voltage change rate of surge pulse by the help of the formula C = Q / U = dQ/dt / dU/dt:
I = dQ / dt = C x dU / dt = 1nF x 2kV / 1.2µs = 1.67A
With a stray capacitance of 10nF the diodes must withstand a current 16.7A. So, the 1N4001 should work. The 1N4001 has the advantage of a very small junction capacitance which can be useful because the diode clamp is sitting in the feedback loop of XTR115 between pin 3 and pin 4.
Eventually, an additional diode clamp made of two antiparallel BAV99 cross pin 2 and pin 3 can be helpful.
If this scheme does not help, you need to redesign your circuit. Please keep in mind that the XTR115 is just not designed to have any connection to outer world at pin 2 and pin 3. All the input circuitry is expected to be supplied by the internally generated supply voltage coming out of pin 8, only.
Kai
Thanks for the advice. We we are working on implementing the diode solution on products in the field while working on a new design. I am not in a position to give further feedback now.
Hi Kai,
We are carrying out some tests. I will give you feedback in due cause.
Thanks