Hi, I'm trying to build a strain gauge circuit using an instrumental amplification IC (INA126PA), however the voltage outputs seem incorrect. Given voltage inputs of V+ = 0.501 mV, V- = 0.500mV and a gain of 5000 (Gain resistor = 18 ohms) I would expect to see about 5V at the output of the chip. Instead I get a value of 0.5V.
Varying the gain resistance or even removing the resistor altogether only has a very small effect on the output (Vo increases by about 20mV), which is what has me really confused.
I've included a circuit diagram below. The circuit is currently built on a breadboard. The input voltages are supplied by a USB NI-6009 DAQ and the input is recorded by this too. I have tried different positions on the board in case of poor connections and I have tried buying another chip in case it was faulty.
I feel like I must be missing something obvious. Can anyone identify a problem?
Regards,
Tim