Hi Team,
I believe OPA2604 is operable under single supply V+=45V, V-=0V (GND) condition.
Is my understanding correct?
I would like to confirm just in case.
Best Regards,
Yaita / Japan disty
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yaita,
Zak is correct in his response but I would like to bring to your attention that due to current quality issue with OPA2604, it now ships only under the waver specifying that the maximum total supply voltage should not exceed 40V instead of 48V specified in the datasheet. This quality problem should be fixed in the next few months at which point OPA2604 will meet again maximum supply voltage limit of 48V (or +/-24V).