Other Parts Discussed in Thread: ISO1540, ISOW7844
Hi team,
The customer is using INA226. The schematic is in the attachment. VBUS pin is not used and it is floating.
The load is the 14K resistance R1. Rshunt is RA1 and it is 0.07ohm. The current that is measured is 7.1mA.
JA1 is a relay. If the voltage is add to 11 pin and 14 pin, the internal switch of the relay will be closed.
For INA226, the Calibration Register value is 0x0725. The Mask/Enable Register value is 0x0003.
Case 1: 100V is connected to IN1 and OUT1 is connected to GND. The internal switch of the relay JA1 is closed.
Then the Shunt Voltage Register can be get the voltage and the voltage is 0.07ohm x 7.1mA = 0.497mV.
The Mask/Enable Register is 0x000B. The Calibration Register value is 0x0725. For case 1, it is fine.