Part Number: PGA205
Hello,
Regarding to PGA205, my customer is asking some question.
Currently, they are checking PGA205 on their board and face noise issue.
(Please refer below.)
They confirmed other frequency(14kHz,20kHz) in addition input signal(17kHz) at ADC output by frequency analysis(FFT) .
To making clear to cause , they confirmed following.
(1) They configured PGA205 gain(x1,x2,x4,x8) by A0/A1 pin and confirmed ADC output data.
(Result)
Input signal(17kHz) -> The signal is output with each gain multiplier(x1,x2,x4,x8).
14kHz/20kHz -> Regardless of gain multiplier, the signal is output approximately 1 time(x1).
From above result, they think it possible that noise issue(14kHz/20kHz) won’t be occurred from the front stage of PGA 205.
(2) They confirmed noise on only ADC block by frequency analysis.
(ADC input -> GND: R312 Removed. C316 shorted to GND.)
(Result)
They couldn’t confirmed two noise(14kHz/20kHz) and input frequency(17kHz).
(Question)
Could you please give us comment, points or advice?
Is there any possible causes?
Regards,
Tao2199