Part Number: OPA388
Hello E2E community,
In a recent project i am using the OPA388 as an Integrator.
The output pin is connected to a 150pF capacitor and a high resitance resistor in parallel to it.
The other side of the capacitor is connected to the negativ input pin.
My problem is, that there is a osccilation at round about 370kHz at the output pin even without an input signal.
Is this the frequency of the internal charge pump or any other component, or is it a problem in my setup?
When disconnecting the power to the op the signal is gone.
Regards,
Dennis