Part Number: OPA1622
Other Parts Discussed in Thread: OPA1688, OPA1612
I'm currently using the OPA1622 as the output amplifier of a DAC product I'm developing. The sound is really good and the part is quite easy to work with. However, I'm feeding it with +5V and -5V and finding difficult to driver certain types of headphones, as the Hifiman HE-6:
- Sensitivity : 83.5dB/mW
- Impedance : 50 Ohms
And the AKG K-1000:
-
Sensitivity 74 dB/mW
-
Impedance 120 Ohm
However, it has no issues driving the Sennheiser HD800:
- Sensitivity 100.10 dB/mW SPL
- Impedance: 430 Ohm
I understand this is mainly due to sensitivity of those devices. Do you think that by using a device that is rail-to-rail like the OPA1688 will make the situation any better? Are there any advantages of using this part over the OPA1622?
I've seen from previous threads that the 1688 will not put as much power on phones as the 1622. Can you please clarify the capabilities considering these corner case devices?
Thanks!