This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
We are using INA128, Instrumentation Amplifier in our design to measure the voltage across a Wheatstone Bridge - Load Cell.
The load cell output terminals are connected at VIN+ and VIN- terminals of the Instrumentation Amplifier INA128.
We have used 2.5V and a resistor divider with two 12K_0.1% resistors as shown in the attachment, to apply a reference voltage of 1.25V
But when measuring, we see that 1.43V is present at VREF terminal.
Also, this reference voltage is changing whenever the load voltage across the Load cell changes.
Could you kindly help in understanding the variation in reference voltage and if it doesn't remain constant?
We are using the below relationship where we assume Vref = 1.25V.
Vout (V) = ((VIN+) - (VIN-)) * Gain + Vref
Thanks,
Denny
Since the reference pin of INA128 is connected to a difference amplifier, you must run the Vref pin with a low impedance source or Vref will be changing with the input voltage caused by changing current in 40k resistor (SEE BELOW).
Thus, in order for the reference voltage to be constant at 1.25V, you must add a buffer between the resistor divider tab and Vref pin -see below.
Denny,
Since the close-loop output impedance, Rout, of an op amps is a function of the open-loop output impedance, Ro, and a loop gain (), it is very low (Zout<<1ohm); thus, any op amp in a buffer configuration will have a low enough impedance and can be used to drive Vref pin of INA128, and the only other consideration is that it meets the required DC precision like voltage offset. Alternatively, one could use an appropriate reference voltage to drive the Vref pin so long as it can sink and source current - see REF3312 or REF3112 (Vref=1.25V).