Part Number: AMC3301
Other Parts Discussed in Thread: AMC3330
Hi,
I am using AMC3301 for the line to line voltage measurement, but have a few questions related to it as follows,
1). In section 8.2 of AMC3301 datasheet, it is mentioned that the device is used for AC line voltage measurement whereas in the diagram it shows AMC3330 for line voltage measurement. So can you please clarify this? Have attached snaps from the datasheet below.
2). Can you please tell the typical cross current value to be considered for the design? (as I didn't found any related information in the datasheet) And if possible can you also provide the minimum and maximum value of cross current.
3). Want to confirm that is this device suitable for AC Line to line voltage sensing for, 1) For +/- 700V range, 50Hz
2). For +/- 1000V range, 140KHz