Part Number: TLV9054
Hi Team,
One quick question.
I understood that TLV9054 will not get damage when applying beyond 0.5V if the input current is restricted less than 10mA from the following description though, is my understanding correct?
(2) Input pins are diode-clamped to the power-supply rails. Current limit input signals that can swing more than 0.5 V beyond the supply rails to 10 mA or less
In my customer case, two TLV9054 are cascaded, 5V power supply for 1st stage and 3.3V power supply for 2nd stage.
Due to power sequencing, 5V are start up earlier than 3.3V so 0.6V was observed in TLV9054 input pin until starting up 3.3 following up 5V. But the input current is restricted 30k ohm series resister(5V / 30k ohm = 0.17mA). My customer would like to get TI's official comment if this use case met Abs max violation or not.
Regards,
Takashi Onawa