Hi,
I would like to know if the LM1815 is suitable for my application. I want to interface it
to the output of a variable reluctance sensor for use in measuring torque.
The output of the sensor is non-sinusoidal with an output voltage which can vary between 0.75V to 12V peak to peak at a frequency of
approximately 40Khz. The spec for the sensor states that the load impedance should be at least 200k Ohm.
Any assistance in determining if the LM1815 will do the job for me would be much appreciated.
Thanks,
Eliot