Part Number: USB2ANY
Other Parts Discussed in Thread: DS90UB953-Q1EVM
Hello,
I have the same case,I installed the USB2ANY software. But I couldn’t find the TI USB2ANY SDK folder. I only found [USB2ANY.dll] in [c:\Windows\SysWOW64\USB2ANY.dll].
When I run [USB2ANY_SupportInfo.exe], I got the following information in [USB2ANY Explorer API Debug.log] file:
2018-08-24 09:32:01.057 DebugLogging is Enabled
2018-08-24 09:32:01.057 PacketLogging is Disabled
2018-08-24 09:32:01.057 Profiling is Disabled
2018-08-24 09:32:01.058
2018-08-24 09:32:01.058 ################################ SESSION START ################################
2018-08-24 09:32:01.058 Loading C:\windows\system32\USB2ANY.dll (v2.8.2.0)
2018-08-24 09:32:01.058 Loaded by C:\Program Files (x86)\Texas Instruments\USB2ANY Explorer\Bin\USB2ANY Explorer.exe)
2018-08-24 09:32:01.058 SDK path is 'C:\Program Files (x86)\TI USB2ANY SDK'
2018-08-24 09:32:01.127
2018-08-24 09:49:18.792 Logging enabled.
2018-08-24 09:49:18.793
2018-08-24 09:49:18.794 Unloading C:\windows\system32\USB2ANY.dll
2018-08-24 09:49:18.796 ##################### SESSION END 2018-08-24 09:49:18.796 #####################
But ['C:\Program Files (x86)\TI USB2ANY SDK] folder is not available !
is there a link where I can download the SDK and the Examples ?
Thank you for your help.
Aziz