Other Parts Discussed in Thread: ISO124, AMC1200
Is it possible a single +5V supply on the ISO124 by connection VS1- to GND1 and VS2- to GND2 and their respective supplies to +5V, when the input is limited to 0-5V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes but you will have very limited signal swing. This is not a rail-to-rail device. Typical input and output swing performance is 2.5V to each rail so you might get reasonable performance with signals from 2.5V to 9.5V. Tested and assured performance is 5V to the rails (a conservative rating), or 5V to 7V.
Regards, Bruce.
Interesting. Can you suggest a device that would is better suited for this type of application?
Hello John, we've got the AMC1200 in development - this is an isolated 5V opamp with a fixed gain of 8 and an input voltage range of +/-250mV. Feel free to contact me directly in case of interests: arek@ti.com.
BR, Arek