Hello,
Customer evaluated their trial board using TPA2005D1-Q1 as I reported on following URL.
https://e2e.ti.com/support/applications/automotive/f/26/t/488285
Speaker cable is longer than 100mm so they should need LC filter, but their board doesn’t have space.
So they start to consider TPA6211A1-Q1 too.
Please answer following questions.
Q1:
TPA6211A1-Q1 datasheet doesn’t explain any short circuit detection.
I observed output waveform using TPA6211A1 EVM with 0.1uF capacitors are connected at Vo+/Vo- and TPA6211A1-Q1 output normal amplified waveform, so I think TPA6211A1-Q1 doesn’t have short circuit detection.
I want to conform TPA6211A1-Q1 doesn’t have shirt circuit detection.
Q2:
In case of using TPA6211A1-Q1 customer wants to connect 0.1uF capacitor at Vo+/Vo- terminal to GND to enhance ESD endurance.
Does 0.1uF capacitor influence to device operation?
Best Regards.